cancel
Showing results for 
Search instead for 
Did you mean: 

Syrine

borisbritwa13
Associate III
Posted on July 06, 2015 at 18:04

Thanks for the answer. But there is a lot of excess and used DMA. (STM32Cube_FW_F4_V1.6.0\Projects\STM32F4-Discovery\Examples\DAC )

I need a

simple example

generated

in

STM32Cube

triangle

generation

.

void MX_DAC_Init(void)
{
DAC_ChannelConfTypeDef sConfig;
/**DAC Initialization 
*/
hdac.Instance = DAC;
HAL_DAC_Init(&hdac);
/**DAC channel OUT1 config 
*/
sConfig.DAC_Trigger = DAC_TRIGGER_T6_TRGO;
sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;
HAL_DAC_ConfigChannel(&hdac, &sConfig, DAC_CHANNEL_1);
/**Configure Triangle wave generation on DAC OUT1 
*/
HAL_DACEx_TriangleWaveGenerate(&hdac, DAC_CHANNEL_1, DAC_TRIANGLEAMPLITUDE_4095);
HAL_DAC_Start(&hdac,DAC_CHANNEL_1);
}
/* TIM6 init function */
void MX_TIM6_Init(void)
{
TIM_MasterConfigTypeDef sMasterConfig;
htim6.Instance = TIM6;
htim6.Init.Prescaler = 0;
htim6.Init.CounterMode = TIM_COUNTERMODE_UP;
htim6.Init.Period = 500;
HAL_TIM_Base_Init(&htim6);
sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
HAL_TIMEx_MasterConfigSynchronization(&htim6, &sMasterConfig);
HAL_TIM_Base_Start(&htim6);
}

why does not work

my code

?

Generation there but it's not a triangle!!! #stm32f4 #keil #discovery #stm32cube #stm32cubemx
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0