cancel
Showing results for 
Search instead for 
Did you mean: 

porting issue with STM X-CUBE-EEPROM_V2.0.0 Emulated EEPROM application for STM32L476G_Discovery application to STM32L412CBU

VK Verma
Senior

Hi ! 

I am trying to port X-CUBE-EEPROM_V2.0.0 Emulated EEPROM application for STM32L476_Discovery application to STM32L412CBU device and following error appears in the flash_interface.c file 

flash_interface.c(151): error: #20: identifier "SYSCFG_MEMRMP

flash_interface.c(168): error: #20: identifier "FLASH_BANK_2" is undefined

It appears that STM32L412 device only has one flash bank and there is no SYSCFG_MEMRMP register or bit filed in its stm32l412xx.h file.

Please suggest how to configure it for STM32L412 devices.

Thanks in advance!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0