cancel
Showing results for 
Search instead for 
Did you mean: 

Keil uv5 application hangs when I add Large C file and The only way out is "killing" uVision via Windows 10 task manager.

GR.5
Associate II

MCU: STM32L071cz

Application : MDK-ARM essentials version 5.35

 when I try to build large project. The "Build Output" window freezes at a random point in the build. uVision is still responsive but I can't stop the build or quit uVision. The only way out is "killing" uVision via Windows 10 task manager. Does anyone know the root cause for this?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
AMuya.1
Associate II

Have you been able to resolve this? I am having the same issue