cancel
Showing results for 
Search instead for 
Did you mean: 

Firmware for STM32F401CC6

YXidi.1
Associate II

I got an STM32F401CC6 blackpill module.

I tried to upload via Arduino IDE the demo project blink.

After succefull upload the board does not work.It lights only the red led and not the blue one.

Is there any way to recover it?

Thank you ,

Yannis

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

Not really an Arduino forum here.

You should be able to program via SWD/JTAG connection.

If you jumper to boot into system mode, and connect via USB, I'd expect it will come up in DFU mode, and you can program via USB option in STM32 Cube Programmer

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
YXidi.1
Associate II

Thanks for your interest.

I know that it is not an Arduino forum.

I just want to know if there is any way to recover it.

My blackpill has no jumpers.

It has 2 buttons one RST and one BOOT.

I press the BOOT button continiously and the the RST one time and that is the way the board gets into progaming mode.

When i do that my Laptop finds the board but i am not be able to upload anything.

TDK
Super User

> i am not be able to upload anything.

Okay... why not?

If you feel a post has answered your question, please click "Accept as Solution".
YXidi.1
Associate II

My problem solved.

It seems that is something wrong with my Mac Arduino IDE installation or with the drivers for STM32 in Mac.

I Tried to upload something in my Windows 10 laptop and everything is OK.

Thank you for our time and help.