2019-01-21 3:30 PM
Hello everyone,
I am trying to setup FLIR lepton breakout board with the Nucle-F7, and I am having trouble finding examples online.
I am using SW4STM32 from AC6 for IDE and have already downloaded the LeptonSDK library package for 32-bit architecture.
There is a repository (https://github.com/groupgets/LeptonModule/tree/master/software)
that has some examples but one of them (nucleo-f4) uses the mbed online IDE.
Thank you!
2019-01-21 9:34 PM
Read the datasheet, make a list of signals between STM32 and the IR imager.
if 160x120x8bit @ 9 Hz seems to yield less than 2 MHz SPI. (double this if 16 bit per pixel)
I2C bus for control, and I guess some GPIO for control signals.
If there is a driver for it, it's most likely to configure the imager and regenerate the picture as a frame in a 2D byte array. You'll have to use DMA+SPI and as initial step use 4 wire interface (even if MOSI is not connected).
Not sure many forum users have experience in the FLIR IR Imager....
2019-01-22 2:29 PM
Thank you for the response.
As my first dive into the datasheet, I did enable the SPI1 on CubeMx for SPI MODE 3 (CPO= 1 | CPHA =1) . Also, configured the clock frequency ABP1 to 13.5 MHz, as the IR would be flexible from 2.2MHz to 20MHz. Flir uses CCI (16-bit wide)which is like I2C , so I did configure the pins for that too.
It is so unfortunate that there is no application on the STM32 side. Mostly are RasPI.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.