Others: STM32 MCUs related

Find out more about STM32 implementations with external components, discuss use cases, and discover how to use new tools and ST components.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to set VTOR in startup script

I'm using an ST part that has 2 banks of flash memory. I've built a code image for the second bank and downloaded it through the debugger. I've changed the startup script to set the VTOR register to the value needed for the second bank, with the line...

LThal by Associate III
  • 845 Views
  • 1 replies
  • 0 kudos

Resolved! Atollic 9.1.0 and Microsoft Devops connection

As of Monday 2019-01-14 my Atollic 9.1.0 IDE has stopped working with Microsoft Devops as the cloud repo. I use the Microsoft TEE Eclipse plugin from Github, latest version. It's worked very well for the last three months, uploads, downloads, etc. ...

Building STM32-Nucleo demo for position independence.

I'm trying to build the IO_Toggle demo for the STM32 Nucleo board as position independent. I've followed the description given in the Atollic TrueStudio for Arm User Guide (p171), and I still end up with variables and structs having problems. Has any...

LThal by Associate III
  • 906 Views
  • 4 replies
  • 0 kudos

Redirect printf() to COM port

A simple question.I have loaded & run the NUCLEO-F401RE \Projects\STM32F401RE-Nucleo\Examples\UART\UART_Printf example.The project sends printf() to COM.I have cut and paste the __io_putchar(int ch) code into my own project.__io_putchar() does not g...

PRobe by Associate II
  • 1752 Views
  • 4 replies
  • 0 kudos

__RBIT() and Truestudio

I want to reverse the Bits of a unsigned long data that is acquired by serial port. I used __RBIT() function in Attolic Truestudio but it does not work . I found during debugging the ARM_ARCH_7M  is not defined .I compiled similar code in the KEIL , ...

MNoor.10 by Associate
  • 1420 Views
  • 3 replies
  • 0 kudos

pointer above 0x4000

pointer above 0x4000 Hi,Why I cannot use pointer above 0x4000. I have declared array form 0x200023d0 [+6000 32bit], so end about 0x28950a10. I am using STM32F769. Iam getting Failed to execute MI command:-data-evaluate-expression *(pDataVectSourceAdd...

embvis by Associate III
  • 1311 Views
  • 3 replies
  • 0 kudos

C++17 support

Hello,Do you plan to enable C++17 or gnu++17 option in the general setting panel for C++ ?Seems like the already bundled GCC compiler support quite a few of C++17 features, and an update to latest gcc-arm would be nice too.I'm mainly looking for chro...

who to implement HAL_GetTick()

I am trying to find time it takes for a loop, am I missing something ?uint32_t time1 = HAL_GetTick();...unit32_t time= HAL_GetTick( ) - time1;I am using Keil when I add time to watch list I am getting response cannot evaluate. It does not show anythi...

MNapi by Senior III
  • 3805 Views
  • 6 replies
  • 0 kudos