cancel
Showing results for 
Search instead for 
Did you mean: 

what may cause STR711FR2H6 reset ?

hg-chen
Associate II
Posted on June 05, 2008 at 08:29

what may cause STR711FR2H6 reset ?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
hg-chen
Associate II
Posted on June 04, 2008 at 04:29

beside reset pin , what may cause STR711FR2H6 reset?

application in GPS,

there was a time that when GPS module turned on consumes too much power can pull low the reset pin,but after this problem fixed,

the random reset still happens sometimes after the set running for a while.

also note that watchdog disabled!

kaouther
Associate II
Posted on June 05, 2008 at 07:54

A supply voltage drop on the V18 or V18Bkp below the threshold 1.35V (+/- 10%) causes a reset beside the reset pin, the watchdog and the software reset. You may check the power supply stage on the board :o

kleshov
Associate II
Posted on June 05, 2008 at 08:29

An erroneous jump to address zero could have the same effect as a proper reset in some applications.