cancel
Showing results for 
Search instead for 
Did you mean: 

What is power consumption at low clock speeds?

ngm
Associate II
Posted on October 12, 2006 at 09:27

What is power consumption at low clock speeds?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ngm
Associate II
Posted on May 17, 2011 at 09:33

I have been looking a little at the datasheets for the STR9 family.

ST gives a linear formula for the power consumption (1.7mA/MHz). - However, I do not feel assured that this formula is valid at speeds of 4MHz external clock divided by 1024 --> approx. speed of 400KHz core frequency and also if I use the RTC clock for the core.

- Does anyone have knowledge of the possible offset of the mA/MHz formula?