cancel
Showing results for 
Search instead for 
Did you mean: 

What is PLL setting in option byte?

alanlai1
Associate II
Posted on October 28, 2003 at 07:30

What is PLL setting in option byte?

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
alanlai1
Associate II
Posted on October 23, 2003 at 23:48

What is PLL setting in option byte? (also PLLx4, PLLx

Is it need to be define while programming?

anshul
Associate II
Posted on October 24, 2003 at 11:29

PLL is used for generating 4Mhz and 8Mhz frequency. It is enabled using the option byte.

e.g. You can select the Internal RC as the source of clock for your application and then enable the x8 PLL option to generate ~8MHz internal clock.

[ This message was edited by: Ansh on 24-10-2003 15:00 ]
alanlai1
Associate II
Posted on October 26, 2003 at 23:24

is it mean that PLL should always be enable

(just choice x4 / x8 only) ?

when it it diasble?

is it the PLL called ''phase lock loop'' ?

anshul
Associate II
Posted on October 27, 2003 at 11:53

Yes, the PLL is ''phase lock loop''.

No, the PLL should not always be enabled. It needs to be enabled only when you want your Internal clock to be multiplied by 4 or 8.

You should enable the PLL by selecting PLL enabled in the option byte and you should select whichever option you require x4 and x8.
alanlai1
Associate II
Posted on October 28, 2003 at 07:27

Thank you very much!!!!!!!!!!

alanlai1
Associate II
Posted on October 28, 2003 at 07:30

Thank you very much!!!!!!!!!!