cancel
Showing results for 
Search instead for 
Did you mean: 

Viper318HD

Rahmaa
Visitor

 

I have  design Buck  converter with Viper318HD ,With below specification:

Vin:(85 to 265)VAC

Vout=12VDC

Iout=500mA

And i not follow recommended   Commponents   value  which  Are mentioned in Edesign tool,  i use  components which  are availble  with me.

So  i need:

1- Know is this  design  will  be stable  to use it  or not ??

 

Rahmaa_0-1762881720207.png

 

1 REPLY 1
Rahmaa
Visitor

when  entered  Input voltage with 265VAC  in Edesign  suit   for operating  condition  for Buck converter  with Viper318HD Controller, 

It mentioned in

1- Ton section

" Cycles skip"

2-IC TJ 300C

 Kindly support us to  Know What mean with these  warings   ,and  are   it will effect on Stability of Circuit  if i operate at 220VAC

Rahmaa_0-1762883332748.pngRahmaa_1-1762883414580.png