cancel
Showing results for 
Search instead for 
Did you mean: 

Using CapCom31 without triggering A/D channel inject on ST10F280

chervenkakirkj
Associate
Posted on October 17, 2003 at 13:36

Using CapCom31 without triggering A/D channel inject on ST10F280

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
chervenkakirkj
Associate
Posted on October 17, 2003 at 13:36

I am coding on an ST10F280 and using both CapCom31 (P7.7) and A/D channel injection. I read that triggering CC31 automatically sets ADCRQ, but I need to find a way to prevent this when I do not want to use channel injection.

1) Is there some way to prevent CC31 from setting ADCRQ?

2) I am presently setting ADCIN (enable channel inject) of the ADCON register right before I attempt a channel inject, and then clearing it immediately after. However, this method still seems to allow one last channel injection before the ADCIN setting takes effect. If I can prevent this, I can get around issue #1. Any ideas?