2005-10-23 3:19 AM
2011-05-17 3:08 AM
I had a rep tell me that the 3300 unit was easier to use for applications where you need to download new code to a unit in the field. He eluded to a change in the memory map logic that made this chip more flexable that the psd813F2 I was using.
Can anyone confirm this? I have looked in the manual but on a quick scan see no difference between the VM reg of a standard PSD part and the uPSD3354D series2011-05-17 3:08 AM
So theres no truth to the claim that flash in program space can be programed? As in the original part, you must have the flash in data space to change it?