cancel
Showing results for 
Search instead for 
Did you mean: 

UART read makes me nuts!

Posted on January 03, 2008 at 12:14

UART read makes me nuts!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on January 03, 2008 at 12:14

Init UART

void init_UARTS_(38400){

UART_InitTypeDef UART_InitStruct;

GPIO_InitTypeDef GPIO_InitStructure;

/*Enable Clock for UART*/

CFG_PeripheralClockConfig(CFG_CLK_UART0 , ENABLE);

CFG_PeripheralClockConfig(CFG_CLK_UART2 , ENABLE);

CFG_PeripheralClockConfig(CFG_CLK_UART3 , ENABLE);

/* Configure the GPIO Tx pins as alternate function push pull*/

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

GPIO_InitStructure.GPIO_Pins = RS485_Tx_Pin;

GPIO_Init (GPIO6, &GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pins = UART2_Tx_Pin + UART3_Tx_Pin;

GPIO_Init (GPIO5, &GPIO_InitStructure);

// Configure UART RX pins as Tristate TTL

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_TRI_TTL;

GPIO_InitStructure.GPIO_Pins = RS485_Rx_Pin; // + UART3_Rx_Pin ;

GPIO_Init (GPIO6, &GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pins = UART2_Rx_Pin;

GPIO_Init (GPIO5, &GPIO_InitStructure);

/* UART Configuration */

UART_StructInit(&UART_InitStruct); //Initialize Structure with default values

UART_InitStruct.UART_BaudRate = baudrate; // Baud rate value

UART_InitStruct.UART_Mode = UART_Mode_8D ; //Set the UARTx Mode 8 bit Data

UART_InitStruct.UART_Loop_Standard = UART_Standard; //Disable LoopBack

UART_InitStruct.UART_StopBits = UART_StopBits_1; // STOP bits number/

UART_InitStruct.UART_FIFO = UART_FIFO_Enable;

UART_InitStruct.UART_Rx = UART_Rx_Enable; /*enable receive*/

UART_Cmd(UART0, ENABLE);

UART_Cmd(UART2, ENABLE);

UART_Cmd(UART3, ENABLE);

UART_Init(UART0, &UART_InitStruct);

UART_Init(UART3, &UART_InitStruct);

UART_Init(UART2, &UART_InitStruct);

***************

read function

unsigned char read_input_function(){

retries++;

while((UART_FlagStatus(UART0, UART_Flag_RxBufFull)==0) && (retries >0))

retries--;

if (retries == 0){

error_flag = 1;

return RESPONSE_TIMEOUT;

}else{

return UART_ByteReceive(UART0);

}

}

***********

main()

char input[99];

for (i = 0; ((i

input[i]=read_input();

}

********'

Works fine, However after my first read, lets say 70bytes. I send a package again and start the read again but this time the read will only read 16 bytes, sometimes only 1 byte. But i if i stop, reset and run the project from start the read will be complete just like the first time.

It seems illogical and intermittent.

Do you have any ideas?