cancel
Showing results for 
Search instead for 
Did you mean: 

The Problem in SSP0+DMA operation

seawwh
Associate II
Posted on January 30, 2007 at 12:56

The Problem in SSP0+DMA operation

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
seawwh
Associate II
Posted on May 17, 2011 at 09:35

The Problem in SSP0+DMA operation

I want to use DMA for both SSP0's RX and TX at the same time

I use the DMA Channel1 for SSP0 RX and DMA Channel2 for SSP0 TX, SSP0 is master mode

1. In SSP0 looptest mode, the following code is OK.

SSP_LoopBackMode(SSP0,ENABLE);

Start_SSPO_RX_DMA(BuRx,20);

Start_SSPO_TX_DMA(BuTx,20);

Or

SSP_LoopBackMode(SSP0,ENABLE);

Start_SSPO_RX_DMA(BuRx,20);

Start_SSPO_TX_DMA(BuTx,20);

2. Connect MOSI and MISO together, the following code is OK.

Start_SSPO_RX_DMA(BuRx,20);

Start_SSPO_TX_DMA(BuTx,20);

or

Start_SSPO_TX_DMA(BuTx,20);

Start_SSPO_RX_DMA(BuRx,20);

3. Connect MOSI and MISO to a peripheral, the following code is OK.

Start_SSPO_TX_DMA(BuTx,20);

Delay_us(10);

Start_SSPO_RX_DMA(BuRx,20);

4. Connect MOSI and MISO to a peripheral, the following code is Error. Why ?

Start_SSPO_TX_DMA(BuTx,20);

Start_SSPO_RX_DMA(BuRx,20);

the result are:

BuRx[0] is a unknown data;

BuRx[1] is the same as BuTx[0];

BuRx[2] is the same as BuTx[1];

... ...

/----------------------------------------------------------------/

#define DMA_Tx DMA_Channel3

#define DMA_Tx_No 3

#define DMA_Tx_ENABLE DMA_Tx->CCNF |= 0x00000001

#define DMA_Tx_DISABLE DMA_Tx->CCNF &= ~0x00000001

#define DMA_Tx_ACTIVE (DMA_Tx->CCNF & 0x00020000)

#define DMA_Tx_End (DMA->TCRISR & (1<

#define DMA_Tx_WaitEnd while (! DMA_Tx_End)

#define DMA_Tx_ClrEnd (DMA->TCICR = (1<

#define DMA_Tx_ClrErr (DMA->EICR = (1<

#define DMA_Rx DMA_Channel2

#define DMA_Rx_No 2

#define DMA_Rx_ENABLE DMA_Rx->CCNF |= 0x00000001

#define DMA_Rx_DISABLE DMA_Rx->CCNF &= ~0x00000001

#define DMA_Rx_ACTIVE (DMA_Rx->CCNF & 0x00020000)

#define DMA_Rx_End (DMA->TCRISR & (1<

#define DMA_Rx_WaitEnd while (! DMA_Rx_End)

#define DMA_Rx_ClrEnd (DMA->TCICR = (1<

#define DMA_Rx_ClrErr (DMA->EICR = (1<

u16 BuRx[20]={0,1,2,3,4,5,6,7,8,9,10,11,12,13,14,15,16,17,18,19};

u16 BuTx[20]={8,8,8,8,8,8,8,8,8,8, 8, 8, 8, 8, 8, 8, 8, 8, 8, 8};

void init_DMA() {

DMA_InitTypeDef DMA_InitStruct;

DMA_Cmd(ENABLE); // Enable the DMA

// DMA For SSP0 Tx

DMA_Tx_DISABLE;

DMA_SyncConfig(DMA_SSP0_TX_Mask, ENABLE);

DMA_StructInit(&DMA_InitStruct);

DMA_InitStruct.DMA_Channel_LLstItm = 0;

DMA_InitStruct.DMA_Channel_DesAdd = (u32)(&SSP0->DR);

DMA_InitStruct.DMA_Channel_SrcWidth = DMA_SrcWidth_HalfWord;

DMA_InitStruct.DMA_Channel_DesWidth = DMA_DesWidth_HalfWord;

DMA_InitStruct.DMA_Channel_DesBstSize= DMA_DesBst_1Data;

DMA_InitStruct.DMA_Channel_SrcBstSize= DMA_SrcBst_1Data;

DMA_InitStruct.DMA_Channel_FlowCntrl = DMA_FlowCntrl1_DMA;

DMA_InitStruct.DMA_Channel_Des = DMA_DES_SSP0_TX;

DMA_Init(DMA_Tx,&DMA_InitStruct);

SSP_DMACmd(SSP0,SSP_DMA_Transmit,ENABLE);

// DMA For SSP0 Rx

DMA_Rx_DISABLE;

DMA_SyncConfig(DMA_SSP0_RX_Mask, ENABLE);

DMA_StructInit(&DMA_InitStruct);

DMA_InitStruct.DMA_Channel_LLstItm = 0;

DMA_InitStruct.DMA_Channel_SrcAdd = (u32)(&SSP0->DR);

DMA_InitStruct.DMA_Channel_SrcWidth = DMA_SrcWidth_HalfWord;

DMA_InitStruct.DMA_Channel_DesWidth = DMA_DesWidth_HalfWord;

DMA_InitStruct.DMA_Channel_DesBstSize= DMA_DesBst_1Data;

DMA_InitStruct.DMA_Channel_SrcBstSize= DMA_SrcBst_1Data;

DMA_InitStruct.DMA_Channel_FlowCntrl = DMA_FlowCntrl2_DMA;

DMA_InitStruct.DMA_Channel_Src = DMA_SRC_SSP0_RX;

DMA_Init(DMA_Rx,&DMA_InitStruct);

SSP_DMACmd(SSP0,SSP_DMA_Receive,ENABLE);

}

/**************************************************

Start DMA Tx

**************************************************/

void Start_SSPO_TX_DMA(void *Bu, u16 Count) {

DMA_Tx_DISABLE;

DMA_Tx_ClrEnd;

DMA_Tx_ClrErr;

DMA_Tx->SRC=(u32)Bu;

DMA_Tx->CC = DMA_SrcWidth_HalfWord | DMA_ChannelSRCInc | 0x80000000 |

DMA_DesWidth_HalfWord | (Count & 0x0FFF);

DMA_Tx_ENABLE;

}

/**************************************************

Start DMA Rx

**************************************************/

void Start_SSPO_RX_DMA(void *Bu, u16 Count) {

DMA_Rx_DISABLE;

DMA_Rx_ClrEnd;

DMA_Rx_ClrErr;

DMA_Rx->DES=(u32)Bu;

DMA_Rx->CC = DMA_SrcWidth_HalfWord | DMA_ChannelDESInc | 0x80000000 |

DMA_DesWidth_HalfWord | (Count & 0x0FFF);

DMA_Rx_ENABLE;

}