cancel
Showing results for 
Search instead for 
Did you mean: 

TDA7850 replace TDA7388

henrylin
Associate

I installed the power amplifier and replaced the TDA7388 with a TDA7850, but there's no sound after installation. What could be the reason?

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @henrylin, to the community!

  • Why did you replace the TDA7388?
  • If it was because of a defect, how can you be sure that the speakers and the connections to them are working?
  • Did you check the relevant voltages (MUTE, ST-BY, VCC pins)?
  • To be on the safe side, you should also place a 10k resistor from pin 25 to GND, which was not necessary with the TDA7388, but with TDA7850.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.