cancel
Showing results for 
Search instead for 
Did you mean: 

STR912 External Memory Interface reading data

s63801
Associate
Posted on November 15, 2013 at 09:55

Hello, I got a question regarding using the External Memory Interface on the STR912. It is planned to use 16 bit multiplexed addressing so the address&data line is bidirectional. I want to use the interface to connect to a FPGA, and writing works. Because I use an input/output connection there can be problems which could destroy the pins of the FPGA, if it is sending at the same time the microcontroller is sending. So the read process is problematic.

Does the EMI inside the STR912 put the address&data line to high resistance to allow transfer from the FPGA to the Microcontroller?

I already looked into the application note AN2647, but it doesn�t describe the process completely, probably because the EMI is normally used to connect a ''dumb'' SRAM or Flash. Is there more documentation?

Thanks in advance.

#str912-emi-external-memory
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0