cancel
Showing results for 
Search instead for 
Did you mean: 

STR910F Power consumption at low operating speeds

gkicomputers
Associate
Posted on June 15, 2006 at 17:24

STR910F Power consumption at low operating speeds

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
gkicomputers
Associate
Posted on May 17, 2011 at 09:30

My question concerns power consumption at low operating speeds. AC current characterists in the STR910F datasheet indicates 1.7 mA/MHz typical in run mode, can I assume that this is a linear specification down at lower MHz? Having an ARM speced this way is not typical, usually power consumption is given for five or six speeds, and the consumption is not linear curve. Most ARM's that I have dealt with have high leakage at, say 1Mhz, so a large current offset exists, so I am wondering if I run this device at 1Mhz will the typical current still be 1.7mA or some offset + 1.7mA? (with only the 1.7mA/Mhz attainable at high speeds)

thanks