cancel
Showing results for 
Search instead for 
Did you mean: 

Startu32.a51

sbencke3
Associate II
Posted on January 06, 2004 at 20:17

Startu32.a51

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
sbencke3
Associate II
Posted on May 17, 2011 at 11:57

What is the file Startu32.a51 that all exaple code (DK3200_1~DK3200_4) use ? Where their functions are called ? Does I have to set-up something at Keil ?

joseph2399
Associate II
Posted on May 17, 2011 at 11:57

Startup32.a51 is the very first program executed after powering up the device. In this file you can setup initial SFR register values such as prescaler value to ADC, PWM, and USB to slow down the logics, also you can disable the Watch Dog timer so you would not get periodic resets.