cancel
Showing results for 
Search instead for 
Did you mean: 

ST92F150 problem,can you help me ?!

misshyx
Associate
Posted on January 19, 2005 at 08:39

ST92F150 problem,can you help me ?!

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
misshyx
Associate
Posted on May 17, 2011 at 11:36

I used a test program testing my chip .

it's work well on the ST9 HDS2V2 EMULATOR, but it doesn't work in chip.

(power 5V,CRYSTAL SCILLATOR 0.6V,4M).

it's I/O PIN output only 0.3V or so!!!?

can you tell me how to do with the problem ?

kapil
Associate II
Posted on May 17, 2011 at 11:36

Is your Hardware throwing the Correct Reset to the micro?

Check it on Probe

Is the Watchdog hardware or software enabled?

Check Pin No 97.

what is your application?