cancel
Showing results for 
Search instead for 
Did you mean: 

ST7Lite

pichet
Associate II
Posted on May 21, 2003 at 06:49

ST7Lite

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
pichet
Associate II
Posted on May 19, 2003 at 01:37

Hello Anyboby

ST7Lite2 Current

I'm using an ST7lite2 and I need to save as much current as possible without an increase to cost.

The LVD detection is taking 0.2mA - Is there a better solution?

or should I use a external regulator with low voltage detection (But this will add to the cost of the final production)

JOM

itsmejatinus
Associate II
Posted on May 19, 2003 at 12:00

hello,

You can reduce the power consumption by using different power saving modes e.g. halt etc. . Its usage depends up on your application means which peripheral/s you want to use and other configuarations.

[ This message was edited by: Ranjeet on 19-05-2003 15:30 ]
stephanie
Associate II
Posted on May 21, 2003 at 06:49

Don't forget also to configure all the unused I/Os as output at 0, to switch off all the unused peripherals, to switch off the ADC between 2 conversions if you don't need continuous conversions,...