cancel
Showing results for 
Search instead for 
Did you mean: 

ST7FOXA0 simulator bug

fggnrc
Associate II
Posted on July 07, 2008 at 05:03

ST7FOXA0 simulator bug

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
fggnrc
Associate II
Posted on July 07, 2008 at 05:03

The attached STVD 4.0 project shows a bug of the ST7FOXA0 simulator.

According to the stimuli file ''Bug.in'', after 64000 clock cycles there are an input capture and a timebase event.

The corresponding interrupt handlers are correctly prioritized as reported in the datasheet: first the input capture one, then the timebase one.

The simulator bug deals with the missing LTCSR_TBF clearing that the hardware does after a read to LTCSR, which is exactly the intended side effect of the instruction:

BTJF LTCSR,#LTCSR_TBF,IC_End

Since IC_ISR clears LTCSR_TBF LTCSR_TBF while the timebase interrupt request is waiting to be serviced, TB_ISR should not be executed but this does not happen.

Regards

EtaPhi

________________

Attachments :

TbIcBug.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I08H&d=%2Fa%2F0X0000000bU4%2F_KRoRxI1A1mfnHAJcRUmOZKpZ9vsvkzg4bUa0ugZekc&asPdf=false