cancel
Showing results for 
Search instead for 
Did you mean: 

ST7FLite with internal RC-oscillator

wolfgang2399
Associate II
Posted on March 28, 2006 at 06:00

ST7FLite with internal RC-oscillator

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
wolfgang2399
Associate II
Posted on April 26, 2005 at 09:00

Hi All,

I've a special question in using the internal RC-oscillator of the ST7FLite2X.

The manual says:

Internal RC Oscillator

 

In this mode, the tunable 1%RC oscillator is used

 

as main clock source. The two oscillator pins have

 

to be tied to ground.

My question is: What can happen, if I don't connect the two pins to ground? Fact is, that I leave them open - to an alternative option with a quartz - with two 22nF capacitors and can't recognize any fault.

Thanks for any suggestions

WoRo

wolfgang2399
Associate II
Posted on March 28, 2006 at 06:00

I'm launching my question again, hoping that finally one of the so called moderators will bother to give an answer, or any other in this forum is able to do so.

Waiting again and thanks in advance

WoRo