cancel
Showing results for 
Search instead for 
Did you mean: 

st7 SCI Comunication

user
Associate II
Posted on November 27, 2004 at 04:51

st7 SCI Comunication

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
user
Associate II
Posted on November 11, 2004 at 06:11

Hi to all,

I have seen on ST brochure an abbreviation ''SCI'' on ST72264G micro.

Can I use it like a UART comunication with PC (through MAX232) ?

Tanks in advantage!!

MBKS

wolfgang2399
Associate II
Posted on November 11, 2004 at 08:05

Hi MBKS,

I use SCI on the ST72334 and it's easily done with 8bits (7bits+parity). Didn't examine with 8bits+parity but I think it runs as well, certainly a little bit more complicated. The SCI has at least the same features as a good UART.

If you use the MAX232 you should have no restrictions on communicating on any asynchronous serial communications interface you want, even full-duplex.

Regards WoRo

alexis23
Associate II
Posted on November 27, 2004 at 04:51

Hi,

I'm using SCI in the 8+1 bit 38900 baud mode, full-duplex. Works very fine.

I've also used it at 9600 bauds without problem.

As already said you just need a MAX232 or similar part, and the transmission is done without RS232 control signals, only Tx and Rx.

There is an AN about the SCI usage.

[ This message was edited by: alpa on 27-11-2004 09:34 ]