cancel
Showing results for 
Search instead for 
Did you mean: 

ST10F276 Flasher and test programm

p-alain
Associate II
Posted on December 15, 2005 at 18:40

ST10F276 Flasher and test programm

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
p-alain
Associate II
Posted on June 10, 2005 at 11:37

I have modified an old electronic card (for ST10F269) to test the ST10F276. I not able to flash it with ST10FLASHER 2.02B. do you have a flasher for this micro and do you have a small programm (i work with Keil) that i could flash. Fcpu = 64MHz. Thank you

Sorry, has somebody a solution to help me please ?

[ This message was edited by: Pierrot73 on 14-06-2005 11:11 ]

michele239955
Associate II
Posted on June 14, 2005 at 14:41

I guess you have to use a newer version, the latest one is 2.4B.

Bye.

gmeyer
Associate II
Posted on December 15, 2005 at 18:40

We created our own version of boot strap load (BSL) Flasher but we have discovered that is doesn't work for the new ST10F276 - CE version. It works fine on the ST10F276 - CA version.

If the memory is not erased our tool works fine. If we erase memory on the -CE part, we only get a few words into programming before a failure is detected. Could I get some information what I need to do to update our BSL? Do we now have to wait after the erase command or look for additional bit changes?

[ This message was edited by: gmeyer on 20-12-2005 18:26 ]