cancel
Showing results for 
Search instead for 
Did you mean: 

ST10 272b and XRAM2

stephane2
Associate II
Posted on May 13, 2004 at 10:27

ST10 272b and XRAM2

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
stephane2
Associate II
Posted on May 11, 2004 at 14:13

Hello,

We are currently using a ST10 269 and began porting/adapting SW to a 272b.

Can XRAM2 (16Kb) be remapped within 00'8000h-00'BFFFh area ?

Or XRAM2 should be called as Huge only ?

Thanks in advance,

Stephane.
najoua
Associate II
Posted on May 12, 2004 at 06:01

Hello,

Yes, XRAM2 (16Kb) can be remapped within 00'8000h-00'BFFFh area.

On the ST10F272-B, XRAM2 address range is user programmable when enabled .

Although this address range is accessed like external memory, it does not occupy BUSCONx / ADDRSELx registers, but is selected via additional dedicated XADRS3 register which defines the Range Size Selection (16Kbytes in your case so RGSZ=0110) and the Range Start Address (your Start Address= 00'8000h so the Rang Start Address = RGSAD= 80h), then XADRS3 must be initialized with the value 806h.

You will find in attachment the register XADRS3 bits description and a definition of the address areas.

________________

Attachments :

Document.doc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Mn&d=%2Fa%2F0X0000000bY2%2FlIbvrzCTb1TGMGyqpTmZHkVR5TGf5XeRqGhIfxdV38o&asPdf=false
stephane2
Associate II
Posted on May 13, 2004 at 10:27

Thanks a lot.

Stephane