cancel
Showing results for 
Search instead for 
Did you mean: 

SOLDERING REFLOW TEMP. FOR TS555IDTTR

VICTOR1
Associate II

HI Sir / Madam,

 

Is there any documents support for the soldering Reflow temp. ofTS55IDTTR, 

reflow soldering profile or curve chart?

THanks.

 

Best Regard,

Victor Lai

 

1 REPLY 1
Peter BENSCH
ST Employee

STMicroelectronics fully complies with JEDEC, which specifies the soldering profile in standard J-STD-020, currently revision F, that you can download here.

The peak temperature Tc can be found in the device’s Material Declaration (product website, tab Quality & Reliability). For the SO-8 of the TS555IDTTR, Tc = 260°C.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.