2004-09-28 2:49 AM
PROBLEM WITH PRIMARY AND SECONDARY MEMORY
2011-05-17 3:03 AM
I have one application in which I have to used the primary and the secondary memory like program and data space. After recording with the PSD express the code area in both memories, the program doesn´t start correctly. When we load the program in the mode debugger with the uVision 2, the code read, it isn´t equal to the primary or secondary memory, and appears aleatory values 01,02,03,04 etc. The same program with the configuration of the secondary memory like program space is running although appears the problem when the program wants to read in the secondary flash.
someone can help me? thanks