cancel
Showing results for 
Search instead for 
Did you mean: 

problem with ADC of ST10F269

juergen239955
Associate II
Posted on May 30, 2006 at 13:48

problem with ADC of ST10F269

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
juergen239955
Associate II
Posted on May 30, 2006 at 13:48

I have following problem with the ADC of the ST10F269:

I have connected VAREF to 2.5V. When I put a voltage between 0V and 1.35V or between 2.0 V and 2.5V I get the correct values from the ADC but between 1.35V and 2.0V it stays on the value of 1.35V.

Can someone help me?

Regards,

Juergen