cancel
Showing results for 
Search instead for 
Did you mean: 

PCI to LAN bridge in STPC VEGA

granitvt
Associate II
Posted on December 23, 2004 at 13:49

PCI to LAN bridge in STPC VEGA

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
granitvt
Associate II
Posted on November 05, 2004 at 02:20

Hello

I have a STPC VEGA chip - STPCV1JEBC (engineering sample). I cann't to write I/O Base address for LAN controller (register with offset 14h has 0h value always). But I can to write Memory Base address for LAN controller (register with offset 10h has value xxxxx000h). Can I to map registers of LAN controller to the I/O space ?

Best regards.
anouar
Associate II
Posted on December 23, 2004 at 13:49

No, all LAn configuration registers are memory mapped.