cancel
Showing results for 
Search instead for 
Did you mean: 

open drain tolerance

diekieh
Associate II
Posted on April 06, 2006 at 07:53

open drain tolerance

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
diekieh
Associate II
Posted on May 17, 2011 at 11:50

Hi Everyone!

I would like to know what voltages could be tolerated by the PSD module when configured as open drain output. Ie. how high can the port pins be pulled up? I'm specifically referring to pin PC7.

Also, the reset state of the port pins are CMOS (push/pull) input. Isn't it dangerous when the hardware is connected in an open drain configuration which may be pulled to a voltage rail incompatible with the PSD module?

Thanks