cancel
Showing results for 
Search instead for 
Did you mean: 

No interrupt during debugging

denglar
Associate II
Posted on April 29, 2005 at 11:23

No interrupt during debugging

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
denglar
Associate II
Posted on April 29, 2005 at 11:23

Hi,

I'm using the ST72F521R9 (TQFP64) with inDART-STX (+Demoboard) and I found a problem using Timer A interrupts (output compare feature):

I've tested my code with STVD 3.1.1 and all works fine but, if I flash it (using DataBlaze), the TimerA interrupt handler is never called (although the application is running).

Even if I debug it with SofTec STVD 3.0.0 (based on STVD 3.1.0) there's no way to have it working.

Below the option bytes:

[FMP_R] = Read-out protecion disabled

[BIT1] package selection = 0

[VD] = Hi voltage threshold

[CSS] = Enabled

[WDG_SW] = Software

[WDG_HALT] = No reset in halt

[PLLOFF] = PLL disabled

[OSCRANGE] = HS: 8-16 MHz

[OSCTYPE] = Ext source

[RSTC] = 4096 cycles

[BIT15] package selection = 1

Does anyone know why?

Previously, I've already used the same pieces of code (timerA interrupt etc...) in another application, with no problem...

Thanks

Regards

Andrea