cancel
Showing results for 
Search instead for 
Did you mean: 

MCU Selection - SD24 + Load Cell

Sadeen
Associate

I need help with MCU Selection.

The main aim is to replace (STM8s and HX711) Chips in a weight scale project.

So, the MCU should be low in cost, include an SD24 with PGA Gain 128.
It also should include SPI interface.

Note: Load cell maximum weight could be greater than 200kg.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Issamos
Lead III

Hello @Sadeen 

Can you explain more about what exactly you want to do .

Best regards.

II

None of the STM32's have a 24-bit Sigma-Delta. Pretty much every one of the STM32 has multiple SPI buses, or could bit bang one.

Perhaps you can expand on why the current implementation isn't working, and what other features newer parts would add to the final project? Computer connectivity? LCD / User Interface?

MSP430AFE2x3 has a "SD24"

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..