2009-01-03 1:39 PM
2011-05-17 1:00 AM
I have introduced a dead time in the signal generated by the MC controller, just as indicated in the RM. My PCLK is 24MHz, Dead time counter type is 6 bits and value 0xF.
When I checked the waveform with my scope, it appears that the dead time is affected by a random jitter of about 120ns!!! The jitter of the two outputs of the same phase (U in this case) are correlated: when the ''H'' output dedtime is increased, the ''L'' output is decreased. This is a two states jitter (0-120ns). Strange isn't it? Does someone encountered this before?