2023-03-20 12:30 AM - last edited on 2024-08-12 4:55 PM by Andrew Neil
We have the goods part number: M4T28-BR12SH1.
On the goods have the number: 9917W. Is it the lot number or other meaning?
I hope to have your consult because our technician had different ideas on this number.
Solved! Go to Solution.
2023-03-20 1:48 AM
Welcome, @TVinh.1, to the community!
9917W (certainly on the first line) is internal information. Only lines 2 to 6 are relevant for the user:
The last line 6 contains again some internal informaton (aaa bb) and the date code in the form YWW, i.e. the last digit of the production year and the calendar week.
Unfortunately, it is not possible to identify directly from the component the decade in which it was manufactured, as the M4T28-BR12SH has been around since 1999. A "1" could therefore stand for 2001, 2011 or 2021, for example. More precise information can only be found on the label of the packaging with which the part was delivered.
Does it answer your question?
Regards
/Peter
2023-03-20 1:48 AM
Welcome, @TVinh.1, to the community!
9917W (certainly on the first line) is internal information. Only lines 2 to 6 are relevant for the user:
The last line 6 contains again some internal informaton (aaa bb) and the date code in the form YWW, i.e. the last digit of the production year and the calendar week.
Unfortunately, it is not possible to identify directly from the component the decade in which it was manufactured, as the M4T28-BR12SH has been around since 1999. A "1" could therefore stand for 2001, 2011 or 2021, for example. More precise information can only be found on the label of the packaging with which the part was delivered.
Does it answer your question?
Regards
/Peter
2023-03-20 2:12 AM
Hello Peter,
Thank you very much for your immediate consultation. This is very useful information to us.
Thank you.
Vinh
2023-03-20 2:18 AM
You're always welcome, I'm glad to have helped you.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter
2024-08-12 3:51 PM
Date code on M4T28-BR12 SnapHat Timekeeper. I just received 5 pieces and we are testing a prototype.
I understand historically there was a 3 digit code, but the ones I received have 4 digits not three.
The sixth line: MYS 99 2405
Can you help.
-Russ
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.