2025-10-17 3:22 AM
Hi, I am working on the LIS2DH12, I have a problem to the appearance of acceleration data. I'm using full scale of +/- 2g and ODR of 400Hz. When the resolution is either 10-bit or 12-bit, only even number acceleration data is read(all x/y/z axis). The acceleration data is generally correct(but only even number). When resolution of 8-bit is selected, now both even and odd number acceleration data can be read. It shows the same appearance for ODR from 1Hz to 400Hz.