cancel
Showing results for 
Search instead for 
Did you mean: 

is there a way to program a MCBSTR9 without uv3?

michael
Associate II
Posted on September 12, 2008 at 06:50

is there a way to program a MCBSTR9 without uv3?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
michael
Associate II
Posted on May 17, 2011 at 09:55

hello,

is there a way to program an MCBSTR9 without the kind support of uv3? is there an external tool that can do the job? something like FlashMagic but working with ULINK...?

thanks in advance!

ibtissem
Associate II
Posted on May 17, 2011 at 09:55

Hallo,

The are many tools supporting the STR9 device programming.

You can for example use the standalone JTAG programmer/CAPS tool from STMicroelectronics to programm all STR9 device families. The USB/JTAG adaptor working with this tool is RLINK from Raisonance or Flink from ST. For more info about the tool :http://www.st.com/mcu/familiesdocs-101.html

Also you can use RFlasher (SW from Raisonance) to program the STR9 flash memories.

The tools listed above are not for development purpose but only for programming target.

Best Regards,

Ibtissem.

dhoyen
Associate II
Posted on May 17, 2011 at 09:55

Hi,

You can also try the Olimex USB - OCD Jtag adapter,if you board has a JTAG connector (should be the case).

The Olimex JTAG adapter cost 50$, Open OCD is open source, and both is usable to program the FLASH or debug a STR912. I m using this solution, and really happy about the result

Regards.