cancel
Showing results for 
Search instead for 
Did you mean: 

inDart OSC_CLK

itamar_nsu
Associate II
Posted on November 24, 2003 at 09:02

inDart OSC_CLK

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
itamar_nsu
Associate II
Posted on November 23, 2003 at 04:57

Hi,

When i use the internal RC osc, do i need the OSC_CLK line (on PB4 or OSC1) from the inDart connector? is it possible to burn the ST7 without this line? (what happens on the first burn process, before i set the option byte to internal RC? would it work without the OSC_CLK?)

thanks

Itamar
jatin
Associate II
Posted on November 24, 2003 at 09:02

Yes, you need not to use OSC1 pin incase you have selected internal RC as the clock source with option byte enable. Now, for the first burn process it depends what's your option byte settings. If it is internal RC with option byte enable then you need not to connect OSC1 pin. Incase your settings are internal RC with option byte disable then you will have to connect the osc1 line to ICC connector to get the clock.