cancel
Showing results for 
Search instead for 
Did you mean: 

Identify 8-SOIC with marking MZ938 (more likely 0621 or O621)

peterpt
Associate II

I am trying to identify an ST IC with marking MZ938.  It is an 8-SOIC and it is used in a circuit which helps maintain charge on a 24V battery and is fed by a boost switching circuit.  It also has 0621 marked on it.  I assume that's the date code.

1 ACCEPTED SOLUTION

Accepted Solutions

The marking is 062I (with uppercase i) = TL062ID.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

7 REPLIES 7

Please attach a large, clear and in-focus picture of the IC

The MZ938 is likely a production code.

https://community.st.com/t5/analog-and-audio/i-had-a-probleme-in-a-ic-st-mzsu938-if-anyone-can-help-me-with-a/td-p/160341

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Probably STISO621 not sure if wide or narrow body

https://www.st.com/en/interfaces-and-transceivers/stiso621.html

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

peterpt_0-1744250449529.jpeg

That angle gets the printed information.  Let me know if you'd like something different.  Many thanks for your help.

I appreciate the suggestion.  I will trace it out and see if this makes sense.

The marking is 062I (with uppercase i) = TL062ID.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

That makes so much sense.  I'll trace more of the circuit to  verify and get back to you here later today.

Many thanks.

Looks good.  Pin 4 is ground.  Pin 8 is 12 V.  Pins 1 and 7 look credible as outputs.  Again, many thanks for your help.

Best regards,
...Peter