cancel
Showing results for 
Search instead for 
Did you mean: 

i2c slave mode (st92f150CR1)

wkissing
Associate II
Posted on November 24, 2004 at 21:19

i2c slave mode (st92f150CR1)

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
wkissing
Associate II
Posted on May 17, 2011 at 11:36

Good morning to everyone!!

Theseday, i am working a slave mode between two ST9s.

One of ST9 is a master mode and another is a slave mode.

I believe that master mode is working well, becaues i have used it

with some slave devices.

It is problem that ST9(slave mode) does not match slave address (I2COAR1, 7 bit mode)

I want to set a slave address which is 0x08 (7bit mode by I2COAR1)

Please, check files attached below.

#define __I2C_C__

#include ''device.h''

#include ''i2c.h''

static unsigned char i2c_sr1;

static unsigned char i2c_sr2;

static unsigned char *i2c_data;

void I2cInit( void )

{

I2cPortInit();

spp(I2C_PG);

// Set the frequency bits before enabling the interface

I2COAR2 = 0xC0; // I2C Own Address Register 2

// - INTCLK between 14 and 30MHz (24MHz)

// - 7-bit mode

I2CCR = 0x00; // I2C Control Register

// - peripheral OFF

// Init interrupt

I2CISR = 7; // I2C Status Register

I2CIVR = 0x30; // I2C Vector register

// 30h : not used

// 32h : error condition detected

// 34h : data received

// 36h : I2C ready to transmit

I2CIMR = I2Cm_IERRM | I2Cm_IRXM | I2Cm_ITXM;

// I2C Interrupt Mask Register

// - all 3 interrupt sources enabled

// Init I2C config registers

I2CECCR = 0x00; // I2C Extended Clock Control Register

// - CC8-CC7 init (0 !)

I2CCCR = 0x92; // fast mode, 400khz

I2CADR = 0x08; // I2C General Call address

// - general call address to be recognized by the device in slave mode

I2CCR = (I2Cm_PE | I2Cm_ACK | I2Cm_ITE);

I2CCR = (I2Cm_PE | I2Cm_ACK | I2Cm_ITE);

// ENGC bit is cleared

// don't use I2C General Call address

} /* end of I2cInit() */

void I2cPortInit (void)

{

OUT_AFOD( 4, 6 );

OUT_AFOD( 4, 7 );

P4DR |= 0xC0;

} /* end of I2cPortInit() */

void I2cIsr (void)

{

int i;

spp(I2C_PG); // Target I2C control registers page

//Save status registers in static user variables

i2c_sr1 = I2CSR1;

i2c_sr2 = I2CSR2;

// Stop detection bit mask or bus error or ack mask

if ((i2c_sr2 & I2Cm_STOPF) || (i2c_sr2 & I2Cm_AF) || (i2c_sr2 & I2Cm_BERR))

{

I2CCR |= I2Cm_STOP;

}

if (i2c_sr1 & I2Cm_ADSL) //slave mode : EV1

{

*i2c_data = I2CDR; // then send stop bit

}

if (i2c_sr1 & I2Cm_BTF) // EV2

{

*i2c_data++ = I2CDR;

if (i2c_sr2 & I2Cm_STOPF) // EV4

{

I2CCR |= I2Cm_STOP; // then send stop bit

}

}

} // end of I2cIsr

#pragma interrupt I2cErrIsr

void I2cErrIsr (void)

{

save_page; // Save peripheral page pointer before modifying it

spp(I2C_PG); // Target I2C control registers page

I2CISR &= ~I2Cm_IERRP; // Clear Error Interrupt Flag

I2cIsr();

restore_page;

} /* end of I2cErrIsr() */

#pragma interrupt I2cRxIsr

void I2cRxIsr (void)

{

save_page;

spp(I2C_PG);

I2CISR &= ~I2Cm_IRXP; // Clear Receive Interrupt Flag

I2cIsr();

restore_page;

} /* end of I2cRxIsr() */

#pragma interrupt I2cTxIsr

void I2cTxIsr (void)

{

save_page;

spp(I2C_PG);

I2CISR &= ~I2Cm_ITXP; // Clear Transmit Interrupt Flag

I2cIsr();

restore_page;

} /* end of I2cTxIsr() */

:o