cancel
Showing results for 
Search instead for 
Did you mean: 

i2c problem

onurozturk123
Associate
Posted on August 15, 2007 at 06:22

i2c problem

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
onurozturk123
Associate
Posted on August 15, 2007 at 06:22

hello everybody

i have a question about i2c(m24c01) application

i send 24 byte data to eeprom with i2c. i can send first 8 byte to eeprom. after that i try to send second byte but i2c hasn't writen

i generate wait function with for loop.i add wait function between

write(00) and write(08) codes. it's allright.

but i want to do this without wait function . namely i want to polling.

already thanks for help

void main(void)

{

.

.

.

i2ctemp[0]=0x23;

i2ctemp[1]=0x23;

i2ctemp[2]=0x24;

i2ctemp[3]=0x24;

i2ctemp[4]=0x28;

i2ctemp[5]=0x25;

i2ctemp[6]=0x30;

i2ctemp[7]=0x26;

write(00);

write(08);

}

void write(Byte address)

{

I2cTxBytes[1]=i2ctemp[0];

I2cTxBytes[2]=i2ctemp[1];

I2cTxBytes[3]=i2ctemp[2];

I2cTxBytes[4]=i2ctemp[3];

I2cTxBytes[5]=i2ctemp[4];

I2cTxBytes[6]=i2ctemp[5];

I2cTxBytes[7]=i2ctemp[6];

I2cTxBytes[8]=i2ctemp[7];

PBDR=0x66;

WriteEeprom(adres);

PBDR=0x77;

}

void WriteEeprom(unsigned char address)//,unsigned char data)

{

I2cTxBytes[0]=address;

I2cTxPtr=&I2cTxBytes[0];

I2cTxEndPtr=&I2cTxBytes[(Txpacketsize-1)];

I2cMode=1; //TX,mode master sends data to slave

I2c_Status=0;

GenerateStart();

PBDR=0x80;

while(!I2c_Status);

PBDR=0X84;

}

void I2C_It_Func(void)

{

unsigned char Temp;

Temp=I2CSR1;

if(Temp == (EVF|BUSY|MS_SL)) //EV6

{

I2CCR|=PE;

Temp = I2CSR1;

}

if(I2CSR2&AF)

{

PADR=0xFF;

}

if(I2cMode==1) //Transmit data to eeprom

{

if(Temp & SB)

{

I2CDR=SlaveAdr; //SlaveAdr=0xA6

}

else if(Temp&BTF)

{

if(Temp&TRA)

{

if(I2cTxPtr==(I2cTxEndPtr+1))

{

I2c_Status=1;

GenerateStop();

}

else

{

I2CDR=*I2cTxPtr;

I2cTxPtr++;

}

}

}

}

if(I2cMode==2) //Recieve data to eeprom

{

if(Temp & SB)

{

if(RepStart==0)

{

I2CDR=SlaveAdr;

}

else

{

I2CDR=(SlaveAdr|0x01);

RepStart=0;

}

}

else if(Temp&BTF)

{

if(Temp&TRA)

{

if(RepStart==1)

{

GenerateStart();

}

else

{

I2CDR=*I2cTxPtr;

RepStart=1; //Repeated Start signal will be generated.

}

}

else

{

if(!(I2cRxPtr==I2cRxEndPtr))

{

if(I2cRxPtr==(I2cRxEndPtr-1))

{

I2CCR&=~ACK;

*I2cRxPtr=I2CDR;

GenerateStop();

I2cRxPtr++;

}

else

{

*I2cRxPtr=I2CDR;

I2cRxPtr++; //RepStart=0;

}

}

else

{

*I2cRxPtr=I2CDR;

I2c_Status=1; }

}

}

}

}