cancel
Showing results for 
Search instead for 
Did you mean: 

how to program an st62t25c

brancaleg
Associate
Posted on July 01, 2004 at 04:43

how to program an st62t25c

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
brancaleg
Associate
Posted on March 02, 2004 at 11:07

I'm trying to program the st62t25c but never success , I mean that when i use it in the circuit it does not work. Of course i have tried the st62e25c for all the test and with this device every think works properly. Where I make a mistake?

GeB
marco32
Associate II
Posted on March 15, 2004 at 06:16

I've had also the same problem.

The reset vector is'nt correct.

Look at the generated hex code at the last line!

If there is'nt a reset vector, the assembler generated $FFh

The stupid thing is, that the eprom version will works OK, but an OTP not!?

How to solve the problem:

Check your endline of your asm code.

The END command must be followed by an ENTER command.

I guess your reset vector is the last uC command

So if there's no ENTER command after the END command, the assembler ignor the last uC command.

Succes
nlangford
Associate
Posted on July 01, 2004 at 04:43

Hi , as suggested there may be a difference in the reset vector but this is not the root cause of your problem.

If you are using the linker ensure that section P1 is assigned correctly eg

-P0:80-07ff