cancel
Showing results for 
Search instead for 
Did you mean: 

Help on In-Application Programming an STR711

davehigton9
Associate II
Posted on February 16, 2007 at 05:45

Help on In-Application Programming an STR711

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
davehigton9
Associate II
Posted on February 13, 2007 at 10:02

I'd appreciate some help here, please.

I have a Front Panel PCB based on an STR711FR0T6 and interfaced

via USB. I have developed the code with the IAR ARM Kickstart

Kit version 4.41. Everything has been trouble free until I

began to add support for in-application reprogramming.

The entire applcation will be well under 32KB, so the strategy

is to erase the top 32KB of flash 0, gradually programme the

top half from USB, then finally erase the bottom half and copy

the top half to the bottom half. Clearly I can't run the code

from flash 0 while it's doing any of this, so I have used IAR's

keyword __ramfunc to locate all the necessary functions (and all

the functions they call) to RAM.

The problem is that even an attempt to erase the top 32KB of

flash 0 stops the device responding over USB until it is power

cycled.

I have disabled interrupts at the start of the procedure by a

call to EIC_IRQConfig (DISABLE), because there are interrupts

from USB and from the timer (the timer is only used to flash

LEDs) and clearly the interrupt vectors and handlers are all in

flash 0. I re-enable interrupts at the end by a call to

EIC_IRQConfig (ENABLE).

Can anyone suggest what I've failed to do or done wrong?

Dave

kleshov
Associate II
Posted on February 14, 2007 at 06:47

I'm not using the ST standard software library for the STR71x, so I could be wrong about some things.

You only need to make a function __ramfunc if it's executed while a flash erase or write operation is in progress. I looked at the source code for the ST standard software library, and I found only two functions that run during sector erase: FLASH_SectorErase() and FLASH_WaitForLastTask(). Those must be __ramfunc. Besides, don't forget about flash module initialization ('STR7 family Flash programming', revision 4, section 2.3.1 'Executing the first Write operation from RAM'), although it shouldn't affect you.

Try setting some breakpoints with the debugger to see where it goes astray.

Regards,

- mike

davehigton9
Associate II
Posted on February 16, 2007 at 05:32

I found the answer a couple of days ago, but my attempts to reply failed.

The problem was that I kicked off the erase, then used WaitForLastTask

to see if it had finished. WaitForLastTask boils down to checking

FLASH_CR)'s BSY0 bit. Of course, while the erase is going on, the

BSY bits aren't readable; if you try, the result you get is equivalent

to not busy! So I returned from the function, to memory that wasn't

readable. Bang.

My solution was to use:

while (FLASHR->FCR0 & (FLASH_LOCK_Mask | FLASH_BSYA1_Mask | FLASH_BSYA2_Mask));

When I single stepped it under the debugger, there was no problem,

because I single stepped slowly enough that the erase operation had

completed.

Thanks for your help!

Dave

[ This message was edited by: DaveHigton on 16-02-2007 10:02 ]