2009-04-28 6:14 AM
2009-04-28 6:14 AM
Hi guys.
I'm using a ST10F269Q2 and I'm trying to use GPT2 T5 and T6 in the capture/reload mode (page 184 in the user manual) to generate interrupts 4 times faster than they come into my system. I can't however get the generated interrupts in phase with the incoming interrupts. The phase continues to drift. Am I doing something wrong or is there no way to get the two in phase? My init code is as follows: T5CON = 0x1005; T5R = 1; T5SC = 1; T5CLR = 1; T6CON = 0x0003; T6R = 1; T6SR = 1; T6UD = 1; T6OE = 1; DP3_1 = 1; P3_1 = 1; CAPREL = 0x0000; Thanks Neil.