cancel
Showing results for 
Search instead for 
Did you mean: 

function of ENET_RXSTR:DMA_EN

alandras
Associate II
Posted on February 08, 2007 at 13:01

function of ENET_RXSTR:DMA_EN

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
alandras
Associate II
Posted on May 17, 2011 at 09:36

According to the ref.man page 170:

DMA_EN: DMA enable bit

Read/Clear bit: a write with ‘1’ reset to ‘0’ the bit value, while a write with ‘0’ has no effect.

In the 91x_enet.c :

void ENET_Start ( void)

{ u32 value;

/* Force a ENET abort by software for the receive block */

ENET_DMA->RXSTR &=~ DMA_RX_START_DMA_EN;

.....

This, if I'm right clears bit DMA_EN, with no effect ???

Later on page 170:

Notes:

– A DMA_EN 0->1 transition resets the FIFO content and the RX interrupts

(ENET_ISR[15:0]).

– A DMA_EN 1->0 transition forces the DMA to immediately close the transfers

toward the AHB bus and MAC core.

I'm confused!

regards,

Andras