2006-10-19 6:33 AM
2011-05-17 12:32 AM
Hi !
I have a problem with the high and low Byte Signals (Pin 21 and 22). While a write access they show a normal behavier ( EMI_BWR_WRLn goes low at low byte write access, EMI_WRHn goes low at high byte write access, both go low at a 16 bit write access ). But while reading none of the signals goes low. (neither at 8-bit nor at 16-bit read access). So my SRAM does not output data. Somebody with a similar problem ?2011-05-17 12:32 AM
Hi,
EMI_WRHn and EMI_WRLn are only used for write access, when doing read access the EMI uses only EMI_RDn. Best regards, STARM2011-05-17 12:32 AM
Use AND gates for memory (eg. single-gate logic), Low# = RD# AND WRlow#, High# = RD# AND WRhigh#.
You can use spare FPGA if present in your design etc.