cancel
Showing results for 
Search instead for 
Did you mean: 

DSL05-024SC6

schmitta
Associate

Can the surge suppressor DSL05-024SC6 be used as a Bridge Rectifier and what are its limits?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome @schmitta, to the community!

Theoretically, you could actually use the DSL05-024SC6 as a bridge rectifier, but as you have already seen in the data sheet, it is not specified for this.

Now there are two possibilities:

  • you are a maker or hobbyist: use the DSL05-024SC6 for a few milliamps only and up to a peak voltage of 4…5 volts under Vbr, here ~20…21V
  • you are a professional: use it only as a TVS for the intended applications

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.