cancel
Showing results for 
Search instead for 
Did you mean: 

DK900

chollan2
Associate
Posted on July 28, 2003 at 20:24

DK900

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
chollan2
Associate
Posted on May 17, 2011 at 11:55

Hi,

I recently purchased the DK900 Developement kit from

http://eu.st.com/stonline/prodpres/memory/psd/html/dk900bd.htm

I was able to compile and run the samples, but I am having trouble trying to

add to the existing projects.

I added putch() for printf(), so that works. Now, when I add files to the

project to get user input and display a menu.

It compiles just fine, but the LCD display is messed up, indicating

something is wrong.

I have no idea what it could be?

I've never messed with Startup.A51 till now.

They do some memory swapping in Startup.A51

I am wondering why PSDload() and PSDload_Init() in Startup.A51?

EXTRN CODE(PSDload_init, PSDload)

LCALL PSDload_init

LCALL PSDload

EXTRN CODE(psd_init)

I have a function called DoLoop(), which just loops getting input, then

display a menu and run some other function.

I tried to swap PSDload and DoLoop in Startup.A51, but that doesn't seem to

work either.

Any idea what I am doing wrong?

Thanks for your help,

nullhi
joseph2399
Associate II
Posted on May 17, 2011 at 11:55

Please see my email reply!