cancel
Showing results for 
Search instead for 
Did you mean: 

Datasheet / 71x_lib inconsistences

ben2
Associate II
Posted on July 19, 2005 at 05:42

Datasheet / 71x_lib inconsistences

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ben2
Associate II
Posted on July 19, 2005 at 05:42

I have found some inconsistences between the datasheet and the 71x_lib to do with the APB regisiters.

In version 6 of the STR71x data sheet(p338) it clearly states

''Bit 0 controls the peripheral in position 1 (I2C0 for APB1 or XTI for APB2) and so on''.

However if you look at the #define in APB.h these are wrong and start at bit 1

from apb.h v3.0 (latest version on st web site)

/* APB1 Peripherals */

#define I2C0_Periph 0x0002

#define I2C1_Periph 0x0004

#define UART0_Periph 0x0010

#define UART1_Periph 0x0020

#define UART2_Periph 0x0040

#define UART3_Periph 0x0080

#define USB_Periph 0x0100

#define CAN_Periph 0x0200

#define BSPI0_Periph 0x0400

#define BSPI1_Periph 0x0800

#define HDLC_Periph 0x2000

/* APB2 Peripherals */

#define XTI_Periph 0x0002

#define GPIO0_Periph 0x0004

#define GPIO1_Periph 0x0008

#define GPIO2_Periph 0x0010

#define ADC12_Periph 0x0080

#define TIM0_Periph 0x0200

#define TIM1_Periph 0x0400

#define TIM2_Periph 0x0800

#define TIM3_Periph 0x1000

#define RTC_Periph 0x2000

#define WDG_Periph 0x4000

#define EIC_Periph 0x8000

Also the EIC_Periph is placed at bit 15 even though the datasheet would appear to have bit 15 as a reserved bit. Although the discription is not clear as the text doesnt mention bit 15.

from datasheet -

Bit 31:16 = Reserved, must be kept at reset value (0).

Bit 14:0 = Peripheral Clock Disable (14:0)

What happend to bit 15 ?

Perhaps on the next release of the 71x library/datahseet you could correct whichever is wrong.

Ben