cancel
Showing results for 
Search instead for 
Did you mean: 

cant program flash memeory

sovpeople
Associate
Posted on August 13, 2011 at 21:22

Hi all!

sorry for my english

I have str-e912 board from Olimex with str912fw44x. Jtag: arm-usb-ocd. I use openOCD(0.5.0) with GDB

when i'm trying to turn off protection on my str9

monitor flash protect 0 0 7 off

cleared protection for sectors 0 through 7 on flash bank 0

how you can see, its all right, but then if i type command to get protection status

monitor flash info 0

#0 : str9x at 0x00000000, size 0x00080000, buswidth 0, chipwidth 0 # 0: 0x00000000 (0x10000 64kB) protected # 1: 0x00010000 (0x10000 64kB) protected # 2: 0x00020000 (0x10000 64kB) protected # 3: 0x00030000 (0x10000 64kB) protected # 4: 0x00040000 (0x10000 64kB) protected # 5: 0x00050000 (0x10000 64kB) protected # 6: 0x00060000 (0x10000 64kB) protected # 7: 0x00070000 (0x10000 64kB) protected str9x flash driver info

nothing change. Why?i know, that there are two protection level registers in str9, but i can't clear them via jtag, because in the documentation (flash programming manual) i failed to find it's address.

Another example: below i'm trying to load hex file with gdb:

(gdb) load

Loading section .dynamic, size 0x88 lma 0x4000000 Loading section .got.plt, size 0xc lma 0x4000088 Error erasing flash with vFlashErase packet (gdb)

this command includeserasing of flash memory, then i try to erase flash:

(gdb) monitor flash erase_sector 0 0 7
error erasing flash bank, status: 0xff
failed erasing sectors 0 to 7

Any ideas?

All this problems started when i have uncommented in 91x_config.h of ARM Firmware library from ST, source which is responsible for booting form 1 bank, while i load the program in flash bank 0 by gdb . Then there was a problem with halting the processor, but i solved it. And now problem, i've described, occurs.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0