cancel
Showing results for 
Search instead for 
Did you mean: 

BSPI and Fifos

tech9
Associate II
Posted on July 04, 2006 at 06:25

BSPI and Fifos

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
tech9
Associate II
Posted on June 20, 2006 at 12:57

Hello all,

We are currently using the BSPI0 on a STR71, with the fifos on.

The depth is 7 words deep.

The receive interrupt is configured to trigger when the receive fifo is full.

However, it is set when we get only 1 word in it; it seems that both flags are set together (RFNE and RFF, respectively receive fifo not empty and receive fifo full).

Is there something undocumented about those flags?

Additionnally; where are those fifos mapped in memory? Are we only able to see the first word in the BPSI registers?

Thanks for any input!

Tech

stankovic
Associate II
Posted on July 04, 2006 at 06:25

Hi,

I didn't have a time to check STR71x (I am working with STR73x) but as it is same family this should be same.

FIFO is actualy on same address - all 16 of them.

So for reading data from FIFO you can do something like this:

for(i=0; iRXR); }

You are practticaly reading same addres 7 times but every time receiving new byte.

It is same procedure for writing in - you write byte after byte on same address.

I hope this will help.